Technical FAQs

Ask a Question

How can I connect EM6400 meters through ETG gateway with SCADA System (Vijeo Citect V7.xx) , which driver I have to use in Vijeo CItect.

For communicating the Vijeo Citect SCADA with EM6400 meters through ETG100 gateways, you need to use MODNET driver in the IO Device configurations
with Device ID (meter id in your case) for each of the IO Device address field,

If you have more than one ETG100 gateway then you need to use different ports for each ETG device in VJC project explorer settings.


Was this helpful?
What can we do to improve the information ?