Technical FAQs

Ask a Question

We are using Vijeo Citect SCADA Ver 7.20 and while defining the 3D array in local variable we are getting the Error “Array size exceeded”.  

While defining the local variable only the array can be one or two-dimensional. However in cicode the usage of a three-dimensional array is as follows: 

INT ArrayA[4][3][2]=1,2,3,4,5,6,7,8,9,10,11,12,13,14,15,16,17,18,19,20,21,22,23,24 


Was this helpful?
What can we do to improve the information ?