Technical FAQs

Ask a Question

What is the maximum width of lugs to fit the NSX400 and also what is the hole size?

 The max width is 32mm and the hole is 10mm
Details are attached.
Was this helpful?
What can we do to improve the information ?