Technical FAQs

Ask a Question

What is the inner dia of Tesys T LT6CT8001 current transformer.

The LT6CT8001 is supplied with a primary connection spacer which is located in the middle of the CT case and has a 10.8mm hole.
This spacer is used to allow connection with a 800 amps bus bar.






Was this helpful?
What can we do to improve the information ?