Technical FAQs

Ask a Question

What is the difference between the screw clamp terminal and the lug terminal connection in case of GV2ME Motor protection circuit breaker.

The screw clamp terminals and ring lugs terminals are identical in their design. The difference is on ring lugs terminal the screw gets
out of terminals base to allow the lugs to be fitted in. The spring terminal is different in its design and the cables are connected to the top of the product.

On screw clamp or ring lug terminals the cable are connected to top and bottom of product. 
Was this helpful?
What can we do to improve the information ?