Technical FAQs

Ask a Question

Is Blokset copper busbar available for busbar surface treatment in order to prevent it from corrosion.

For Blockset copper busbar it is recommended to have Sn30 busbar surface treatment as it can cover all the copper bar.
While using small thickness there is a risk to have uncoated bubbles that could drive to corrosion.
So as close as 30 microns it is sure to protect busbar from corrosion .
Was this helpful?
What can we do to improve the information ?