Technical FAQs

Ask a Question

How to terminate “Move Velocity” configured as Data set type in Motion Sequence operating mode for Lexium 32M range of servo drive.

While operating Lexium 32M range of servo drive in “Motion Sequence” operating mode, data set type configured as “Move Velocity” can be terminated
only if parameter of respective data set “Transition type” is set to “Abort and Go Next”. Aborting of “Move velocity” will be done as per settings of
parameter “Transition Condition 1”, “Transition Value 1”, “Transition Condition 2” and “Transition Value 2”. Following abortion of “Move Velocity” Data Set
will be followed as per setting of parameter “Subsequent Data Set”.
Was this helpful?
What can we do to improve the information ?