Technical FAQs

Ask a Question

What are the communication port numbers for serial PCI module installed in M258 0r LMC058 controllers.

Maximum 2 numbers of serial PCI modules can be added to M258 logic controller or LMC058 Motion controller.
 
If one serial PCI module is installed then the serial PCI module link is COM2, regardless of the physical PCI slots used. LinkNumber associated with COM2 is 2
 
If two serial PCI modules are installed then the serial PCI module plugged on the left side PCI slots is COM2 and the serial PCI module plugged on the right side
PCI slots is COM3.
LinkNumber associated with COM2 is 2 and LinkNumber associated with COM3 is 5
Was this helpful?
What can we do to improve the information ?