Technical FAQs

Ask a Question

How does One Licensing work for Power Monitoring Expert 7 software

When a Power Monitoring Expert order is processed, Activation ID(s) are created just for that order.  A Software License Certificate containing the activation ID(s) is included in the DVD box and can also be emailed if requested on the purchase order.  After installing the Power Monitoring Expert system, the software must be “activated” using the activation ID(s) from the Software License Certificate in order to use the software features that have been purchased.  “Activation” creates a secure key based on the physical machine and sends this in an Activation Request (xml file) to the Schneider Electric licensing server.  The server registers the activation with that order to a Power Monitoring Expert machine and sends back an Activation Response (xml file) that confirms the activation from the server to the Power Monitoring Expert machine.  The Power Monitoring Expert software modifies its behavior based on whether or not particular licensed features are activated.
Was this helpful?
What can we do to improve the information ?