Technical FAQs

Ask a Question

What is the “Complete” button for in Power Monitoring Expert 7 Floating License Manager

The “Complete” button is used for “web portal” activations if the Response XML file has not yet been loaded into the Floating License Manager.  It is not necessary to “Complete” activations if they are already listed in the Floating License Manager.
Was this helpful?
What can we do to improve the information ?