Technical FAQs

Ask a Question

What is the “Repair” button for in Power Monitoring Expert 7 sortware Floating License Manager

If the PC hardware changes, or other modifications are made to the PC that invalidate it’s unique identifier, a license may become “untrusted” (indicated in the Floating License Manager with an icon next to the license row).  If this happens, the license must be “repaired” in order to be used by Power Monitoring Expert.  The “Repair” button will contact the Schneider Electric license server to refresh the license activation. 
Was this helpful?
What can we do to improve the information ?