Technical FAQs

Ask a Question

We are unable to access HELP file in concept Version 2.6 software with Windows 7 platform    

Please Install the attached file (i.e.Windows6.1-KB917607-x86.msu) in your Windows 7 32 bit machine.

Please make sure Concept SR 7 must be installed prior to installation of above mentioned file, if it is not installed then please install that too.
Patch file Concept Sr7 is attached (i.e.Concept_26_SR7_en) for reference.

Please download the above files from below mentioned link:

https://schneider-electric.box.com/s/spjdz90a5643yi4f8830
Was this helpful?
What can we do to improve the information ?