Technical FAQs

Ask a Question

Is it possible to establish communication over modbus RS422 with TSX ETG100.

Yes it is possible,As there is no setting for modbus RS422 protocol in TSX ETG100 howevevr following Steps explained in below attached file 
will help to establish a healthy communication over modbus RS422 protocol.
 
Was this helpful?
What can we do to improve the information ?