Technical FAQs

Ask a Question

What is ASCII message storage capacity of a 140ESI 06210 module.

The ESI module can hold up to 255 ASCII messages with 127 characters plus checksum character each. These ASCII messages can be
either static texts to be sent to an external device or a definition of how data contained in the register area is to be translated into or from a
stream of serial ASCII characters, or a combination of both.
Was this helpful?
What can we do to improve the information ?