Technical FAQs

Ask a Question

Does Vijeo Citect have a driver supporting to IEC60870-5-101 protocol.

For the driver for IEC870-5-101 in VJC there has been a driver developed by Microsol ( ) named “IEC870t” Citect
driver which is a 32-bit driver that provides communication services for devices that use the IEC870-5-101 Communication Protocol.
Was this helpful?
What can we do to improve the information ?