Technical FAQs

Ask a Question

Which function block in Unity pro can calculate maximum, minimum and average of a Analog Input(Process Variable) in a Batch.

In Unity Pro V7 we have to use Derived Function block  to make custom block for calculating max, min & avg of a analog value in a batch. 
You can make a dfb with code as shown below. Also enclosed is sample dfb file.


Was this helpful?
What can we do to improve the information ?