Technical FAQs

Ask a Question

Does Modicon Quantum platform support IEC60870-5-101 & IEC60870-5-103 protocol .

Yes Quantum platform support IEC60870-5-101  & IEC60870-5-103 protocols . PTQ-101M, IEC-60870-5-101 Master and 
PTQ-103M IEC-60870-5-103 Master are the modules designed to be used on IEC60870-5-101 & 103 protocols. These modules are created, designed
and supplied by ProSoft Technology. These modules are designed to be used in Quantum Standalone systems only.
Was this helpful?
What can we do to improve the information ?