Technical FAQs

Ask a Question

What are the factory default communication parameters shipped with the COM option (BCM ULP)

 The factory default communication parameters shipped with the communication module are :
 
- Address : 47
 
- Speed : 19200 bauds
 
- Parity : even
 
If you need to change above parameters, you have to enter those new parameters, into the communication module,by using the Micrologic Utilities RSU (Remote Settings Utilities).
Was this helpful?
What can we do to improve the information ?