Technical FAQs

Ask a Question

Is it possible to mount base plate which is being used for interlocking of Compact NSX MCCB 100...630A in vertical position.

Yes, base plate designed for interlocking of  2 no's Compact circuit breakers NSX 100...630 can be installed horizontally or vertically on a mounting rail.
Was this helpful?
What can we do to improve the information ?