Technical FAQs

Ask a Question

Is it possible to use MN undervoltage release in combination with C60 MCB and C60 Vigi module.

The interpretation is like that the MCB will be fitted over Vigi module and the electrical auxiliaries like MN undervoltage release are left hand side mounted to MCB.

So this combination is possible.
Was this helpful?
What can we do to improve the information ?