Technical FAQs

Ask a Question

Can the scale factor be manually changed on the Series 200, 700 Power Meter to display more resolution on the display

The Series 200, 700 Power meters do not have a command interface that allows the user to change the scale factors.  The scale factors are automatically determined based on the CT and PT ratios.
Was this helpful?
What can we do to improve the information ?