Technical FAQs

Ask a Question

What is the function of the bar which is available inside the LT6CT8001 & how to install this CT with this bar.

 The LT6CT8001 should be delivered with service instruction and normally all information should be present. 
 
The bar which is delivered inside this CT is design to handle the current flow through the CT. You can not remove this bar. 
 
Please find the the catalog extract and pictures showing the LT6CT8001 in the attachment and how to install bar on. 
Was this helpful?
What can we do to improve the information ?