Technical FAQs

Ask a Question

What is the withstand internal temperature values of PCB and internal parts for Tesys T relay.

The LTMR controller monitors its Controller Internal Temperature, and reports warning, minor fault, and major fault conditions. Refer below the withstand values for the withstand internal temperature ;
Major internal temperature fault (at 100 °C / 212 °F) 
Minor internal temperature fault (at 85 °C / 185 °F). 
Was this helpful?
What can we do to improve the information ?