Technical FAQs

Ask a Question

What is RM6 closed type CT? How to install RM6 Closed typeC.T. on RM6 isolator bushings?

 
The Close CTs are the current acquisition module for the instalation on the interface module which are special RM6 feed-through. 
 
In fact the closed CT is dedicated to RM6 cubicle for T200 application. 
 
This closed CT to be installed near the bushing at the back of the metallic plate. The diameter of this CT is about 80 mm. 
The reference of this CT is AF-T200-TFxx (SOR9921). Refer the attached file for the details.
 
 
Was this helpful?
What can we do to improve the information ?