Technical FAQs

Ask a Question

Is RM6 suitable for mining application?

Yes, RM6 can be used in the marine application as per the technical specification of RM6. 
Please refer the attached one file having the advantage & various customer project including mine application. 
Was this helpful?
What can we do to improve the information ?