Technical FAQs

Ask a Question

What is the contact material for power contacts of LC1D series contactor.

The material of the Tesys D range power contacts are : 
 
- LC1D09/12/18 and CAD : AgNi (Silver and Nickel). 
- LC1D25/32/38/40/50/65/80/95/115/150 : AgSnO2 (Silver and Tin oxide). 
 
Was this helpful?
What can we do to improve the information ?