Technical FAQs

Ask a Question

How to do factory default setting (Master Reset) including the IP address of EGX100, EGX300.

A master reset to an Ethernet Gateway (EGX) will reset all settings to the factory default settings including the IP address.  For the EGX100 and EGX300 the default IP address is  You can use Modscan software or some other Modbus TCP/IP program to send the master reset.  For the EGX100 and EGX300 use address 254 and write decimal 9030 to register 2800. Once you have sent this register command to the EGX you will have to cycle power to reboot the processor.
Was this helpful?
What can we do to improve the information ?