Technical FAQs

Ask a Question

How to resolve an error message "SFTCommon Library is not installed in this system" while running CET850 software.

Unfortunately, the CET850 software does not come with those SFTCommon-... files. You should be able to correct this by downloading another piece of software that we have called "SFT2841" that can be found at below link :
Installing SFT2841 will install the SFTCommon-ICDLibrary and SFTCommon-SCLSchema. 
When asked for a Serial Number for SFT2841, use '0647740-08' or '8888888-06'. 
Once you have installed SFT2841, these errors should go away. Make sure you have the CET850 software closed when doing the SFT2841 installation. 
Was this helpful?
What can we do to improve the information ?