Technical FAQs

Ask a Question

What is the purpose of CET850 software and where can i download the same.

Purpose: CET850 is used for the advanced configuration of the IEC61850 communication. Some basic configuration can be done using SFT2841, but CET850 offers a lot more functionalities for the communications configuration. Please note, the configuration of the Sepam behavior can only be done using SFT2841, so both programs are useful for advanced configurations.
Download link:
Was this helpful?
What can we do to improve the information ?