Technical FAQs

Ask a Question

What is a Acti 9 Reflex iC60.

The Acti 9 Reflex iC60 is a circuit-breaker which combines in a single device to have the function of remote control of an installation and the protection functions of a circuit breaker.
Was this helpful?
What can we do to improve the information ?