Technical FAQs

Ask a Question

Does the Acti 9 Reflex iC60 allow reclosing upon a fault.

It is not possible to reset the Reflex iC60 remotely upon a fault, because the Reflex iC60 is designed for resetting to be performed manually after a repair operation on the fault (fault cleared).
Was this helpful?
What can we do to improve the information ?