Technical FAQs

Ask a Question

What are the Acti 9 C60H-DC circuit breaker mechanical and electrical operating cycles.

The Acti9 C60H-DC circuit breaker mechanical and electrical operating cycles are:

Mechanical : 20,000 cycles

Electrical : 3,000 cycles (where L/R=2 ms) 
                    6,000 cycles where the circuit is resistive
Was this helpful?
What can we do to improve the information ?