Technical FAQs

Ask a Question

Is there any cuttable Comb Busbar available for circuit breakers in Acti 9 range of products.

Yes, the cuttable Comb Busbar is available for circuit breakers in Acti 9 range of products.

Functions:
 
> Can be sawn and cut in a single pass, using busbar chocks
> Supplied with two IP20 lateral end-pieces except for 57 module references
> The end-pieces are compulsory during cutting
> The phases are identified by symbols on each side of the comb busbar
> Cutting marks on the insulating material
> The spare teeth can be insulated with tooth covers
Was this helpful?
What can we do to improve the information ?