Technical FAQs

Ask a Question

Is it required to provide an isolation in each side of Acti 9 C60NA-DC direct current switch-disconnector.

Yes, It is recommended to provide a Spacer clips of 9 mm in each side to provide isolation for Acti 9 C60NA-DC direct current switch-disconnector.

The ordering code for 9 mm spacer is 27062.

Also, a terminal Screw Shield is recommended to snap onto the front of the C60NA-DC protective devices to provide greater insulation of the terminal screws.

The ordering code for Terminal Screw Shield is 26981.
Was this helpful?
What can we do to improve the information ?