Technical FAQs

Ask a Question

Is it possible to have changeover system when two Compact NS1600b-3200 MCCBs are interlocked using rod or cable connection.

It is not possible to have changeover system by using two Compact NS1600b-3200 MCCBs by means of interlocked using rod or cable connection.
The interlocking by cable or rod is only available with two Masterpact NW air circuit breaker above 1600A.
Was this helpful?
What can we do to improve the information ?