Technical FAQs

Ask a Question

Is 140DDO35310 Source or Sink type digital output module.

140DDO35310 is True low Output 24 Vdc 4X8 Sink Module. The 24 Vdc True low 4X8 Sink module switches 24 Vdc, and is capable of driving displays logics and other loads up to 500 mA sinking in the ON state.

Was this helpful?
What can we do to improve the information ?