Technical FAQs

Ask a Question

Can i configure BMXNOM0200 as a modbus slave when installed in QERIO X80 drop.

The BMXNOM0200 can be used in a X80 drop managed by a "performance" BMXCRA i.e BMXCRA31210 to access modbus slaves, or any other device using the "character" mode. All the other characteristics of NOM are maintained except the support of Modbus slave and modem management.
Was this helpful?
What can we do to improve the information ?