Technical FAQs

Ask a Question

How to modify the logging measurements of 2- and 3-phase measurements after enabling the displaying of 2- and 3-phase measurements of BCPM in ION Enterprise 6 or Structureware Power Monitoring 7 Vista.

You can use MDI "Configure Logging and Calculation" tool to open the BCPM translator file if you need to modify the logging of the measurements for 2- and 3-phase data logging.
Note :  Refer FA177056 - How do enable the displaying of 2- and 3- phase measurement of BCPM in ION Enterprise 6 or Structureware Power Monitoring 7 Vista.
Was this helpful?
What can we do to improve the information ?