Technical FAQs

Ask a Question

The PowerLogic BCPM or BCPMSC shows 0A on every circuit, even though the panel the meter is monitoring has a load. The meter has been installed correctly and all CT connections are made.

If the ribbon cables are reseated while the BCPM is on, the unit will not register current. 
The BCPM does a discovery of the ribbon cables only upon bootup. 
If the ribbon cables are reseated or seated after bootup, the BCPM will not detect the current.
Was this helpful?
What can we do to improve the information ?