Technical FAQs

Ask a Question

What are the available configurable communication parameters in BCPMSC.

Communications Configuration:  Communications parameters for the BCPMSC are field selectable for your convenience. Please see attached Figure 14 for selector location.
The following parameters are configurable:
 Baud Rate:  9600, 19200, 38400
 Parity On or Off
 Parity:  Odd or Even
 Wiring:  2 or 4 wire RS-485

Was this helpful?
What can we do to improve the information ?