Technical FAQs

Ask a Question

What is the recommendation for cabling and connection in Round ribbon and Flat ribbon cable used in PowerLogic BCPM.

Round ribbon cable is recommended for use when the BCPM printed circuit board will be mounted outside of the PDU that is being monitored. 
Round ribbon cable is the prefered choice when the ribbon cable will be threaded through conduit.

Flat ribbon cable is recommended for projects where the BCPM printed circuit board will be installed inside of the PDU that is being monitored.
Flat ribbon cable is more flexible than round ribbon cable and is the preferred choice if the ribbon cable will not be threaded through conduit.

Was this helpful?
What can we do to improve the information ?