Technical FAQs

Ask a Question

Is it possible to use the current sensor strip from one Branch Circuit Power Meter (BCPM) model (A/B/C) to another

It is possible to interchange the CT strips, but it is recommended to use the current sensor strips that came with the unit and are therefore calibrated together.
Otherwise, the error LED will illuminate on the BCPM Circuit Board. The serial numbers of the circuit board and sensor strips are encoded together. If the BCPM senses that the serial numbers do not match, the error LED will illuminate.
Was this helpful?
What can we do to improve the information ?