Technical FAQs

Ask a Question

Can i format M340 CPU SD card using windows.

One can not format the M340 memory card with a non-Schneider tool. The memory card needs a structure to contain program and data. Formatting with another tool or windows destroys this structure. Also you should not use a write-protected memory card with the module. Some services do not operate properly when the memory card is write-protected.
Was this helpful?
What can we do to improve the information ?