Technical FAQs

Ask a Question

Can i use the same BMX RMS*** SD card in the CPU and the NOE module.

The SD cards for BMX CPU & NOE have different memory structures and you can not replace these cards with one another. There are three different part numbers for CPU & NOE modules based on the features & services they include relating to Monitoring,Diagnostic, Setup & FactoryCast.

NOE 0100 :- BMXRWSB000M
NOE 0110 :- BMXRWSFC032M
Was this helpful?
What can we do to improve the information ?