Technical FAQs

Ask a Question

Which elementary functions can be performed by communication and fieldbus master DTM

A communication and fieldbus master DTM can provide the following functions:
•Field device discovery
•Communication diagnostics
•Gateway and communication configuration
•Automatic generation of the I/O Scanning lines for data exchange between the PAC and the device
•Fieldbus master configuration (fieldbus master)
Was this helpful?
What can we do to improve the information ?