Technical FAQs

Ask a Question

Can i configure Physical link for Channel 1 of NOM0200.2 as RS232.

BMXNOM0200.2 is equipped with two channels: Channel 0 and Channel 1 – Only Channel 0 can be configured using either a RS232 line or a RS485 line, while Channel 1 is a RS485 line only.
Was this helpful?
What can we do to improve the information ?