Technical FAQs

Ask a Question

How much memory is consumed for the DTM information in PAC controllers

A DTM in Unity Pro can be divided into two parts: The executable part & The data part.
The executable part of a DTM is not included into the Unity Pro program and cannot be transferred into the PAC. Therefore, the executable part does not use any memory area in the Unity Pro program. Hence, all required DTMs must be installed before opening the Unity Pro project.  Unlike the executable part, the data may be optionally included in a Unity Pro program. The memory area occupied by the data of the DTMs is the Upload Information area.
Was this helpful?
What can we do to improve the information ?