Technical FAQs

Ask a Question

How to enable a io channels for Time Stamping on a X80 drop

In Unity V7 Data Editor three new columns are added relating to time stamping. Using these you can enable time stamping to a partcular IO channel. Below is a description:    
  • Time Stamping :  Activates the Time Stamping on the variable 
  • Kind of detection : None, Raising Edge or Falling Edge, Both Edges. These values could be modified by the user (in case of ERT module this value can be modify in the ERT screen too. The ERT module and Data Editor will notify each other)
  • Source : Indicates the source of the Time Stamp >>  When selected CRA : comes from a BMX Drop,  ERT: comes from an BMX ERT module
  • ID : Unique ID associated to the Time Stamped variable (except for the ERT in Applicative mode where the ID is the channel number)
Was this helpful?
What can we do to improve the information ?