Technical FAQs

Ask a Question

How do I determine the default IP address of ETZ410/510 Ethernet module

The first 2 octets of the ETZ410/510 module's default IP address is always 85.16. The last 2 octets of the default IP address of the ETZ410/510 module is derived from the last 2 numbers of it's MAC address by converting Hexedecimal values to decimal.

For Example:
The module's MAC address is (in HEX): 00 80 F4 01 29 C3
The default IP address (in decimal) would be:   ( where 29 Hex = 41 Dec  and C3 Hex = 195 decimal )

Was this helpful?
What can we do to improve the information ?