Technical FAQs

Ask a Question

Is it possible to automatically discover devices in the Profibus DP network using PRM module

The devices connected to a Profibus DP network via PRM can be auto discovered using Fieldbus discovery. The fieldbus discovery  feature is available in the PRM master DTM (UNITY) and in the COMM DTM ( for third party tool). Using this feature from Unity terminal itself you can scan all the profibus devices connected to the PRM module.
Was this helpful?
What can we do to improve the information ?